Por favor elija país e idioma:

B&R sponsors the successful Austrian Eco-Racing team

With their innovative "Fennek" vehicle, students from the Technical University of Graz presented an energy-efficient concept car that uses an absolute minimum of fuel. Comprehensive testing on the rolling friction test stand – equipped with B&R technology – made it possible to optimize running resistance and ensured continual improvement in power usage. "Fennek" made waves during the Shell Eco-marathon 2011 competition at the EuroSpeedway in Lausitz with a result of 843 km/kWh while exhibiting maximum energy efficiency.

In 2010, the Fennek achieved 1,773 km/liter (gasoline equivalent); this year the Fennek achieved 7,495 km/liter, representing an efficiency increase of over 300%. In addition to 1st place in the "Plug-in" category, the Austrian Eco-Racing team also won the CO2 evaluation.

Active project support

As a long-time partner of the TU Graz, B&R supports students in the implementation of many different types of projects. In addition to providing the absolute latest automation technology, the company's engineers are also standing by to assist with technical expertise. "We want young engineers to become familiar with our technology as early as possible," explains Thomas Dicker, the project supervisor from B&R. "When they begin their own careers later, it's possible that they will recall their experience with B&R components when developing their own solutions."

Por favor elija país e idioma:

B&R Logo