• Sitio web
  • Referencia
  • Número de serie
Iniciar sesión
Conectado comoNombre de usuarioCerrar sesión
Cargando...
B&R Logo

Boosting the sustainability of linear movements

ACOPOSmicro and LinMot

An increasing number of pneumatically implemented motion solutions are no longer competitive. Tubular linear motors have proven to be a much more efficient solution. In applications with frequent, short linear movements, these motors reduce energy consumption and CO2 emissions by over 90%. NTI and B&R are paving the way for a smoother transition to this more sustainable drive technology. The LinMot linear motors sold by Swiss manufacturer NTI can be controlled directly using ACOPOS servo drives from B&R.

In the musical Starlight Express, electricity wins the race between the various types of drive technology. The machine manufacturing industry shows a similar trend towards fully electric solutions. One of the many reasons for this is the motivation to reduce the energy consumption of production lines. Conventional approaches to improving energy efficiency have already harvested all the low-hanging fruit, however.

The efficiency that remains to be gained through improvements to standard drive technology has been reduced to mere percentage points. To achieve any kind of significant reduction in energy consumption and CO2 emissions, designers need to think a little further outside the box. Railroad technology provides a perfect analogy.

In the 1970s, in spite of immense infrastructure costs, the electric drive replaced steam traction, which uses locally generated steam to drive the cylinders. These engines were horribly inefficient. Although the exhaust steam was generally reused in auxiliary and secondary systems, these measures brought only marginal improvements in the overall energy balance.

Enormous energy losses with hydraulic drives

The pneumatic cylinders widely used in industrial machinery operate on the same fundamental principle as the cylinders of a steam engine. They are used to implement frequently repeating linear movements with short, constant paths. Despite countless improvements to the details of this technology, the overall system efficiency leaves much to be desired. Simply generating the pressurized air in the (usually electric) compressors accounts for 80 percent of the total energy consumption – before the cylinders have performed any work whatsoever. Additional losses are incurred as the air makes its way to the cylinder.

A study conducted by the German research organization Fraunhofer shows an average of 25% additional energy lost due to leakage in pipes and valves. With a hydraulic drive, braking energy can't be regenerated; decompressed air is released into the atmosphere instead. The overall efficiency of a pneumatic axis is therefore less than 10%.

Tubular linear motors – The cost-effective alternative

NTI_LinMot #3
The higher purchasing price of tubular linear motors compared to pneumatic cylinders begins to be balanced out by the reduced complexity of the circuit.

A considerably more efficient alternative to the pneumatic cylinder is a linear motor, which uses electromagnetic forces to convert electrical energy directly into movement. A convenient side effect of linear motors is that, since they lack fluid components, they are much easier to install. This is especially relevant in cases where short linear movements are the only aspect of the machine that use pneumatics.

Like all electric motors, linear motors are extremely efficient by nature. This fundamental efficiency can be further increased using advanced drive technology such as ACOPOS servo drives from B&R, which can store braking energy in a DC bus circuit to be used for later acceleration. It is also relatively simple to return excess energy back into the power grid.

Most linear motors are optimized for applications with more extreme demands on dynamics and precision, however. When it comes to very simple movements, replacing a pneumatic solution with a linear motor solution is not cost-effective. The tubular linear motor, however, is indeed a practicable alternative to the compressed air axis. The stator on a tubular linear motor is located inside a tube, wrapped around the magnets of an armature rod. Its simplified, symmetrical design make it easier to produce than the more well-known flat or U-shaped linear motors. It is cheaper, easier to use and lasts longer while providing the same active power.

Cost reduction from 3,000 to 100 euros

NTI_Blumer Ernst

"The potential for a real leap in energy savings was brought to our attention by a customer for whom we were calculating the energy consumption of our motors in comparison to a pneumatic system," explains Ernst Blumer, head of sales at NTI AG, manufacturer of LinMot linear motors and servo drives. "This customer needed to move a 15 kilogram load a distance of 400 millimeters at a rate of 30 cycles per minute. According to our calculations, savings of over 90 percent were possible. These savings have been confirmed by measurements taken on the actual system. In this particular application, the energy cost per axis was brought from 3,000 euros per year down to only 100."

NTI_LinMot #1
Only three years after being introduced to the market, the linear motor driven model of the pick-and-place handler developed by German manufacturer electropneumatische Systeme GmbH outsells its considerably lower-priced pneumatic counterpart by 50%. (Source: NTI)

Replacing the pneumatic cylinder, which is similar in size and shape, can dramatically reduce the energy consumption of linear axes and provide an exceptionally fast return on investment. The reduction of CO2 emissions is also impressive. In three-shift production, the pneumatic axis in this application emits over 12 tons of CO2 – the equivalent of driving 100,000 kilometers with a modern mid-sized car.

B&R paves the way for a smooth transition

Eder Bernhard

"It is especially important to us to see our customers benefit from more sustainable solutions," says Bernhard Eder, product manager at B&R. "We were able to make use of the shift in technology for linear movements in an easy way and integrate this concept into the entire system." B&R's ACOPOSmicro servo drive thus has an encoder interface for LinMot's 80 VDC series tubular linear motors as a standard component. The Swiss manufacturer's 3x 400 VAC series is already equipped with ACOPOSmulti-compatible encoders.

ACOPOSmicro
ACOPOSmicro servo drives come standard with a LinMot encoder interface for 80 V tubular linear motors, while the 400 V models are controlled by ACOPOSmulti drives.

Aside from the enormous energy savings, tubular linear motors offer some remarkable functional advantages as well. They can perform several billion strokes before failure, so there is never a need to replace a cylinder. This not only lowers maintenance costs, but and reduces downtime as well. Tubular linear motors are also well-suited for high frequency applications such as textile machines. Pneumatic drives are incapable of providing the necessary 600 strokes per minute with precision in the hundredth of a millimeter range, nor do they have the necessary durability. Standard linear motors, on the other hand, are too expensive.

Precision down to the hundredth of a millimeter

Integrated position measurement provides contact-free positioning with a precision down to 0.05 millimeters without causing mechanical wear. For applications requiring even higher precision, an additional external position encoder can bring the precision into the micrometer range. Integrated sensors send data such as the current stator temperature to the controller for diagnostics and condition monitoring.

The biggest procedural advantage comes from the freedom with which movements can be configured. Stroke length, velocity, acceleration and force can be programmed flexibly. B&R's ACOPOS line of servo drives can be used to implement highly complex movements over the entire stroke, allowing the axis to be adapted to changing conditions, such as workpiece size, or used for synchronized parallel movements with third-party axes.

ROI after only 5 months

NTI_LinMot #2
The higher initial costs are recovered quickly thanks to the radical energy savings. In one pick-and-place application, the investment was recovered after only five months. (Source: NTI)

To this day, the well-known pneumatic and hydraulic technologies continue to dominate when it comes to linear movements. The reason? For machine manufacturers looking at initial investment alone, these solutions appear less expensive than electric drive technology. "With continuously rising energy costs, however, customers purchasing production machines learned long ago to view total cost as the top criteria," says Blumer. Over a production line's entire service life, it can easily become much more expensive to rely on outdated technology like pneumatics and hydraulics. "In the handling application we mentioned, the higher initial costs were recovered in only five months thanks to the reduction in energy costs, and after two years they're looking at savings of nearly 6,000 euros," continues Blumer. "Large, innovative machine and systems manufacturers are already having the power and air consumption of their machines certified in order to provide their customers a realistic picture not only of the investment costs, but also the operating costs of a system."

"In addition to energy consumption, replacing hydraulic and pneumatic systems with linear drive technology can also reduce the cost of development, construction and commissioning," adds Eder. "B&R's ACOPOS line offers customers a uniform solution for all types of motion control tasks. They stand to substantially increase the energy efficiency of their machines – whether they use a stepper, torque, synchronous, AC or DC motor or replace a pneumatic axis with a linear drive." And regardless of the task at hand and what type of drive technology is used to accomplish it, B&R's Automation Studio provides a universal development environment for all aspects of motion control.

Automation Studio_Logo

Automation Studio has a full selection of powerful, integrated tools for positioning tasks. Even the most complex movement sequences can be realized without tedious programming. IEC 61131-3 compliant PLCopen motion control function blocks help simplify and streamline development of motion control applications.

Ejemplo
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Privacy Policy.