• Sitio web
  • Referencia
  • Número de serie
Iniciar sesión
Conectado comoNombre de usuarioCerrar sesión
Cargando...
B&R Logo

Safe programming in Automation Studio

25.09.2012
BuR_PR12032_SafeDesigner
SafeDESIGNER 2.90 gives users a clear and comprehensive overview of all modifications to a project.

Graphical project comparison with SafeDESIGNER Version 2.90

Eggelsberg – New and improved SafeDESIGNER Version 2.90 is now available from B&R. As an integral component of the Automation Studio development environment, SafeDESIGNER ensures safety and reliability when programming sensitive functions for the protection of equipment and personnel. All modifications to safety systems are completely protected by a restrictive change process. In this new release of SafeDESIGNER, a helpful graphical view has been added to the comparison function. Users now have a clear and comprehensive overview of all modifications to the safety system. The effects of changes to safety functionality can now be localized even faster and more effectively.

The project comparison in SafeDESIGNER 2.90 makes it possible to determine which verification and validation procedures are required based on well-founded information and to analyze differences between machine generations. Projects don't need to be compiled before they can be compared, either. SafeDESIGNER 2.90 lets users compare even unknown or temporary uncompiled software versions.

SafeDESIGNER draws some of its components from the open technology platform of the Safety Alliance. "The Safety Alliance is an association of leading automation manufacturers, service providers and users of safety technology – including B&R – who benefit from the synergy of their various areas of expertise," explains Peter Fuchs, Spokesman of the Safety Alliance. Its mission is to promote the marketing and continuous development of an open technology platform for functional safety based on the market standard from KW-Software. The manufacturer-independent certified technology components are already being used in solutions from countless leading automation suppliers. The platform's open, modular and scalable architecture greatly simplifies the development, integration and application of functional safety technology. Para más información, visite www.br-automation.com

Acerca de B&R

B&R es una compañía de capital privado con sede en Austria y oficinas en todo el mundo. Como líder mundial en automatización industrial, B&R combina la tecnología de vanguardia con una avanzada ingeniería para proporcionar a los clientes de prácticamente cualquier industria soluciones completas para la automatización de máquinas y procesos, control de movimiento, HMI y tecnología de seguridad integrada. Con estándares industriales de comunicación de bus de campo como POWERLINK y openSAFETY, además del potente entorno de desarrollo de software Automation Studio, B&R está constantemente redefiniendo el futuro de la automatización. El espíritu innovador que mantiene a B&R al frente de la automatización industrial está impulsado por el compromiso de simplificar los procesos y superar las expectativas del cliente.

Para más información, visite www.br-automation.com

Si vuelve a imprimir esta nota de prensa, envíe una copia a:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg

BuR_PR12032_SafeDesigner
Download
Download
Ejemplo
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Privacy Policy.