To be able present your project, you need to develop a project concept. We have a clear vision of how this should be done and require that you prepare your project according to our guidelines. For a project presentation, you need a poster and a short description that represents the basic requirements for a successful presentation.

Short description

Short description

The first thing you should do is write a short description of your project. You will surely refer back to it often during the process of completing the project. The following information must be included:

  • The project concept – How did the idea for the project originate?
  • What is special about your project? What makes it challenging or difficult?
  • What is your proposed solution and how do you plan to implement it?
  • Which B&R hardware is needed?
  • [Mandatory information: Name, Adviser, Educational institution, Project name]

Poster

Poster

The poster is a visual representation of your project concept. Use colors and symbols – inspire the viewer! The following information must be included on the poster:

  • Project title
  • Project designers
  • Project advisor
  • Educational institution
  • Sketch of the machine or system
  • Connections between the B&R hardware and the machine or system
It is not at all about how the poster or presentation looks, dealing with the project topic is more important. It is necessary to show the important characteristics and special features of your project to those watching the presentation.

Presentation

Presentation

It is easy to notice if a presentation was poorly prepared, even after a lot of practice. Here are some helpful guidelines and tips:

  • You have 5 minutes – Having less time available for a presentation means that more work is involved in preparation.
  • Speak loudly and clearly.
  • Maintain eye contact with your audience.
  • Think about what you are doing with your hands.
  • Be sure the topic is clear. What is the goal of your project?
  • What makes your proposal interesting?
  • Why is your project such an awesome idea?
  • What are the benefits of your solution?
  • How do you plan to implement your project?
  • Don't forget about the target group.

Please choose country and language

B&R Logo