• Website
  • Model Number
  • Serial number
Login
Logged in as UsernameLogout
Loading...
B&R Logo

B&R keypad module with E-stop

09.24.2013
e-stop key pad
The robust B&R keypad module with E-stop is available in three designs: black, glossy black and white.

Decentralized machine operation – Easy and safe

B&R's illuminated ring keypad modules with IP65 protection are designed for installation directly on the machine. First introduced in early 2012, the latest addition to this series is a model that includes an integrated E-stop button. With both the button and the electronics integrated in a low-profile housing and standard M8/M12 connectors, installation and wiring are about as easy as it gets.

Easy installation, easy integration

These control devices can be mounted anywhere on the machine at intervals of up to 100 meters. Installed using only two screws, they require no additional accessories and can easily be connected to any common bus system. The signals for the E-stop button can be connected directly to a safety circuit or incorporated via SafeIO modules into an integrated safety network such as openSAFETY.

Ergonomic machine operation

B&R E-stop keypad modules meet the most stringent requirements for ergonomics and are extremely easy to clean. With no surface edges, indentations or grooves, these modules are perfectly suited for use in hygienic applications as well. In addition to providing tactile feedback, the illuminated ring keys ensure an even distribution of light for clear signaling and can also be labeled individually.

About B&R

B&R is a privately owned company with headquarters in Austria and offices all around the world. As a global leader in industrial automation, B&R combines state-of-the-art technology with advanced engineering to provide customers in virtually every industry with complete solutions for machine and process automation, motion control, HMI and integrated safety technology. With industrial fieldbus communication standards like POWERLINK and openSAFETY as well as the powerful Automation Studio software development environment, B&R is constantly redefining the future of automation engineering. The innovative spirit that keeps B&R at the forefront of industrial automation is driven by a commitment to simplifying processes and exceeding customer expectations.

For more information, visit www.br-automation.com.

When reprinting this press release, please send a copy to:

Bernecker + Rainer Industrie-Elektronik Ges.m.b.H.
Corporate Communications
B&R Strasse 1
A-5142 Eggelsberg
Austria, Europe

e-stop key pad
Download
Download
Ejemplo
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Privacy Policy.