• Website
  • Materialnummer
  • Seriennummer
Login
Eingeloggt als BenutzernameAusloggen
Laden...
B&R Logo

Innovation Day B&R UK & Ireland

header_Innovation Days UK

As the world becomes more and more connected, machine and factory automation solutions from B&R are empowering manufacturers to new levels of productivity. Join us for a day to experience these solutions and technologies first hand and discover how you can apply them to your machine or factory as we journey through the fourth Industrial Revolution

We aim to educate and entertain through a variety of seminars that are grouped in three core areas: 1) Automation State of the Art, 2) Innovations, 3) Industrial Internet of Things (IIoT). By having various speakers from B&R UK & Ireland, B&R Austria, and partner companies, you will be exposed to a range of new ideas to incorporate into your machine or factory. This includes a demonstration of B&R's Supertrak complete with openROBOTICS using Comau Robots and B&R's Orange Box.

register-now-click-here-button-hi

What to expect on the day

B&R will install exhibition style demonstration units and product walls to facilitate discussions during the coffee breaks and throughout lunch. We aim to expose the participants to the latest technology developed by our team of innovation experts as well as through sharing through a group of selected customer case studies presented directly by them.

The day is bisected by lunch and an optional tour of Jaguar's Castle Bromwich Site.

As a bonus, we will also be raffling off 3 tickets to Jaguar's Performance Comparison Experience which will give you the opportunity to drive both the F-TYPE and XE on the same course.

Reception.4
Jaguar Visitor Centre Reception Area
SuperTrak II (compact)
B&R's Supertrak with Comau Robotics

Seminar Schedule

We aim to educate and entertain through our seminar sessions with topics grouped in three separate blocks: 1) Automation State of the Art, 2) Innovations, 3) Industrial Internet of Things (IIoT).

A mix of speakers from B&R UK&Ireland, B&R HQ in Austria, and our partners will present to the audience.

  • Time
    Session
    Topics
    8:00-9:30
    Registration/Tea/Coffee
    Exhibition Area
    We will have product and demonstration units available and sales and applications engineers available to speak with during this time.
    9:30-9:35
    Opening Statement
    Conference Room
    Industrial Automation: The Heart of Industry 4.0
    9:35-10:30
    Session 1: Automation State of the Art
    a) Scalability+ (20min) + Smart Maintenance Solutions
    B&R is an innovator and leading supplier of automation solutions for industrial applications. Not only do we excel in HW design but also SW design to allow the users of our technology to have a truly scalable automation platform for their machines and factories.
      
    b) Case Study: ATM Automation BuildAssist (20 min)
    ATM Automation based in Leicester has been a long standing machine builder using B&R in a variety of their solutions for the Automotive, Food, Plastics, and Medical Industries. With the help of B&R’s scalable HW and SW, ATM’s BuildAssist range is able to accommodate 100s of possible solutions so that their customer gets exactly the support required for the application.
      
    c) Mechatronics by B&R (20 min)
    B&R has a reputation for fast PLCs, but what about our motion expertise? ATM Automation bought the very first ACOPOS drive in the 1990s, so how does the ACOPOS P3 now stack up? We will also explore some of our Mapp functions and how we can enable our customers to get motion applications up and running fast to leave time for their software designers to spend their time adding value in other non-routine tasks.
    10:30-11:15
    Tea/Coffee Break
     
    11:15-12:30
    Session 2: Innovations
    a) Case Study: MappVIEW & TSM Controls (25 min)
    TSM Controls based in Dundalk Ireland, were searching for a solution to modernise their line management solution in time for launch at the K-Show in Germany last year. B&R’s mappVIEW provided them with the look and feel along with the flexibility they required to make it happen.
      
    b) Human-Robot Collaboration at EngRoTec (20 min)
    A systems integrator has provided us with a unique comparison between a classical robotic cell system and one using openROBOTICS. This sessions will look at the unique benefits such as reduce shop floor space and a higher integrity solution that allows HRC to be successfully implemented with normal high payload robots from Comau.
      
    c) B&R Supertrak Demonstration (25 min)
    As the manufacturing environment continues to look for marginal gains in productivity, areas of planned downtime, such as product changeover time, have become targeted. This requires a higher level of flexibility that can be offered by B&R’s linear transport system, Supertrak.
    12:30-14:30
    Lunch
    Exhibition Area + Optional 45 Minute Tour of Jaguar’s Manufacturing at Castle Bromwich
    14:00-15:30
    Session 3: Industrial Internet of Things (IIoT)
    a) IIoT Introduction (10 min) Data is being used to gain competitive advantages now across all industries and within the factory, we call this the Industrial Internet of Things. Why do we care and how can we take advantage of this growing segment within industrial automation to lock in marginal gains that enable us to compete in a global market place.
      
    b) Case Study: AutoCoding Systems Ltd. (20 min)
    The AutoCoding solution automates the set-up of packaging line devices to avoid coding errors and with the use of barcode scanning verifies that the packaging is always correct for all products. The risk of product recalls due to coding or packaging errors is therefore greatly reduced. AutoCoding specialise in the integration of packaging line devices. As industry leader in packaging line automation solutions, they have a complete understanding of the complexities of packaging line processes.
      
    c) The Power of the Digital Twin for a Systems Approach to Machine Design (30 min)
    A Digital Twin can have several benefits including the ability to run in-line with the real machine to enable rapid task-planning and early detection of potential problems. By integrating a Digital Twin of the machine design on a real-time platform as a Functional Mockup Unit (FMU), the virtual machine can be configured and tested in parallel with the real machine to accelerate the commissioning process, reduce risks and decrease costs.
      
    d) Case Study: Nestle and the Orange Box (20 min)
    How is worlds largest food manufacture applying the tools made available from the IIoT revolution? Combining resources with B&R, Nestle is on the path to realising true growth by improving their OEE and Asset Intensity metrics with the Orange Box; a revolutionary technology that allows existing assets to be digitised in less than 1 hour.
    15:30-16:00
    Closing Statement
    Closing + H&S for Factory Tour + PPE
    Seminar Schedule with Details

Partners

We welcome you to the home of the Jaguar Experience and not only do you have the opportunity to learn about B&R, but also hear directly from some of our partners including:

ATM Automation (www.atmautomation.com)

ATM Automation designs and manufactures robotic and automation systems for the Automotive, Medical, Plastics and Packaging industries. With a heritage spanning over 40 years ATM has established a solid reputation for innovation, engineering excellence and unprecedented levels of customer support.

ATM Logo

AutoCoding Systems (autocodingsystems.com)

The AutoCoding solution automates the set-up of packaging line devices to avoid coding errors and with the use of barcode scanning verifies that the packaging is always correct for all products. The risk of product recalls due to coding or packaging errors is therefore greatly reduced.

AutoCoding specialise in the integration of packaging line devices. As industry leader in packaging line automation solutions, they have a complete understanding of the complexities of packaging line processes.

Autocoding logo

Comau (www.comau.com)

Our product range extends from small payload robots to the massive capacity of 650 kg. The robot team available for our clients is wide, well known and appreciated. We provide articulated industrial robots suitable for any application and special robots for spot and arc welding, palletizing or press to press automation.

Each of our robots is designed with a reduced footprint, large work envelope, highly precise movements and positioning, greater reliability and low maintenance costs.

Comau Logo

Fronius (www.fronius.com)

As world market leader for robot welding and technological leader worldwide for arc- and resistance spot-welding the Division Perfect Welding has a mastery of the entire spectrum: MMA, TIG, MIG/MAG, plasma and LaserHybrid.

Fronius_logo

TSM Control Systems (www.tsm-controls.com)

From the cap of your toothpaste tube to the milk carton on your breakfast table or the plastic bag that you buy your vegetables in, you’ll find that TSM has played a vital part in the manufacturing process.

For almost 40 years, we’ve been supplying blending and control systems that enable companies to achieve the level of precision that their production processes demand, operating within a spirit of trust, compliance and fairness that has become our hallmark.

Our blueprint for success is based on three core planks: Innovation, People and Experience – each of them feeding into a single vision of being the world-leader in gravimetric blending and controls.

TSM logo
Ejemplo
Share
Um Ihnen benutzerdefinierte Einstellungen auf br-automation.com bereitstellen zu können, speichert B&R Informationen über Ihren Besuch in sogenannten Cookies. Durch die Nutzung dieser Webseite erklären Sie sich mit der Verwendung von Cookies einverstanden. Informationen über den Einsatz von Cookies erhalten Sie in unserer Datenschutzerklärung.