Vælg venligst land og sprog

Deterministic timing is achieved by applying a cyclic timing schedule for all connected nodes to access the physical layer. The schedule is divided into an isochronous phase and an asynchronous phase. During the isochronous phase, time-critical data is transferred; the asynchronous phase reserves bandwidth for non time-critical data. The cycle sequence is controlled by the managing node (MN) in the real-time domain. The MN frees access to the physical medium via explicit messages. As a result, just one single node has access to the network at all times, thereby preventing collisions. The CSMA/CD mechanism, which causes non-deterministic Ethernet behavior, has no effect when POWERLINK operates free of disturbances.

POWERLINK uses MAC addressing in accordance with IEEE 802.3. Each device has a unique MAC address. In addition, nodes in the real-time domain are assigned an EPL node ID. The respective node ID of a device can be selected by a node switch on the front side of the device. Ethernet POWERLINK also offers standard IP addressing when needed. This means that real-time devices can be accessed from anywhere in the world via the Internet. Local IP addresses are assigned to devices in a real-time domain. The local IP address for a particular device is derived from the respective node ID. The transition to the Internet is made via Network Address Translation (NAT), as when connecting to an Internet service provider.

Vælg venligst land og sprog

B&R Logo