2014-09-02
A development computer [1] that must fulfill the following hardware requirements:
A target system [2] that must be one of the B&R automation devices released with Windows Embedded Standard 7:
with:
The development computer must be running one of the following operating systems:
and must have the following software installed:
Modify the the Windows Embedded Standard 7 image for your needs.
For a detailed description of the Windows Embedded Standard 7 development process see:
Windows Embedded Standard 7
http://msdn.microsoft.com/en-US/library/ff795587(v=winembedded.0).aspx
You will find following topics on this page:
You can also consult a Windows Embedded Standard Training from a Microsoft Training Partner. Search the Microsoft Website http://www.microsoft.com for Windows Embedded Partner Search or Windows Embedded Classroom Training.
[1] The development computer is the
computer where you install the Windows Embedded Standard 7 Toolkit.
[2] The target system is the
computer where you run Windows Embedded Standard 7.
[3] You can download the Microsoft .NET
Framework from the Microsoft Web site
http://www.microsoft.com.
[4] You can download the Microsoft
Core XML Services (MSXML) from the Microsoft Web site
http://www.microsoft.com.
[5] You can download an evaluation version of Windows Embedded Standard 7
SP1 (= Toolkit) from the Microsoft Web site
http://www.microsoft.com.
[6] The B&R Windows Embedded Standard 7 BSP contains
all files specific for B&R automation devices and can be downloaded from the B&R
Web site http://www.br-automation.com. For this download a customer login on B&R website is required.
[7] The Image Configuration Editor (ICE) is part of
the Windows Embedded Standard 7 Toolkit and can be used
to create or modify an answer file.
[8] The answer file defines all the files, packages and drivers
that the Windows Embedded Standard 7 image should contain. It can be used to
create a bootable setup medium that installs the image on a target system. Answer
files for B&R automation devices are included in the B&R
Windows Embedded Standard 7 BSP.
[9] You can download the B&R Windows Embedded Standard 7
Development Guide from the B&R Web site http://www.br-automation.com. For this download a customer login on B&R website is required.