------------------------------------------------------------------ File: Readme.txt Version: V1.3 Date: 2011-01-13 Description: B&R Windows CE 6.0 PP300/400 ------------------------------------------------------------------ Below you will find a short description and version information of the software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ This is the B&R Windows CE 6.0 version for B&R Power Panel 300/400 devices. ------------------------------------------------------------------ INSTALLATION ------------------------------------------------------------------ For further informations, see the Windows CE 6.0 help. The help can be downloaded from the B&R homepage www.br-automation.com. ------------------------------------------------------------------ Version V1.3 / 2011-01-13 / PAM ------------------------------------------------------------------ Fixes - Videos could not be played because necessary components were not included in the image. - Various USB flash drives did not work, including the B&R USB flash drive 5MMUSB.2048-01. - Updated with ELO touchscreen driver 2.00. The previous version of the the touchscreen driver could enter an endless loop trying to resynchronize after communication error. Symptoms ranged from communication failure to apparent system crash. - Updated with B&R control panel applet "Touchscreen" 3.8. This version does not reboot the device if the user cancels the control panel applet. Changes - Used CE 6.0 updates: * Windows Embedded CE 6.0 R3 * Winodws Embedded CE 6.0 Product Update Rollup 2009 * Windows Embedded CE 6.0 Update 100131_2010M01 * Windows Embedded CE 6.0 Update 100228_2010M02 * Windows Embedded CE 6.0 Update 100331_2010M03 * Windows Embedded CE 6.0 Update 100430_2010M04 * Windows Embedded CE 6.0 Update 100531_2010M05 * Windows Embedded CE 6.0 Update 100630_2010M06 * Windows Embedded CE 6.0 Update 100731_2010M07 * Windows Embedded CE 6.0 Update 100831_2010M08 * Windows Embedded CE 6.0 Update 100930_2010M09 - B&R HMI Diagnostics 1.2 added. - B&R Zip 1.0 added. - B&R ADI SNMP Agent 1.0 added. - Updated with B&R ADI 1.25 - Updated with B&R AutoRun 5.2 - Updated with B&R CleanScrean 3.0 - Updated with B&R Configuration Manager 3.3 - Updated with B&R Control Center 1.33 - Updated with B&R Image Viewer 1.2.1 - Updated with B&R PVI 3.0.0.3116 - Updated with B&R Registry Editor 3.5 - Updated with B&R Screen Capture 1.0.2 - Updated with B&R Screen Saver 2.4 - Updated with B&R Task Manager 2.1.1 - Updated with B&R VNC Viewer 3.13 - The USB Drivers (EHCI.DLL und USBDISK6.DLL) have been updated with all Microsoft QFEs up to july 2010 (Update 100731_2010M07). - Component WMV/MPEG-4 Video Codec added. - Component Windows Media Technologies added. - Component ASX v1 and M3U File Support added. - Component ASX v2 File Support added. - Component ASX v3 File Support added. - Component NSC File Support added. - Component Windows Media Multicast and Multi-Bit Rate added. - Component Windows Media Streaming from Local Storage added. - Component Windows Media Streaming over HTTP added. - Component Windows Media Streaming over MMS added. - Font Arial Bold Italic added. - Font Comic Sans MS Bold added. - Font Courier New Bold added. - Font Courier New Bold Italic added. - Font Courier New Italic added. - Font Impact added. - Font Times New Roman Bold added. - Font Times New Roman Bold Italic added. - Font Verdana Bold added. - Font Verdana Bold Italic added. - Font Verdana Italic added. - The Windows style was changed to standard. - The desktop wallpaper was removed. ------------------------------------------------------------------ Version V1.2 / 2009-05-04 / HOH ------------------------------------------------------------------ Changes - Execution time of large applications improved. - Component XML Mime Viewer added. - XML files associated with Internet Explorer. - Component PCL Printer Driver added. - Component Animation Control added. - All "Locales" added. - Used CE 6.0 updates: * Windows Embedded CE 6.0 Product Update Rollup 2008 * Windows Embedded CE 6.0 Update 090131_2009M01 * Windows Embedded CE 6.0 Update 090228_2009M02 * Windows Embedded CE 6.0 Update 090331_2009M03 - B&R Screen Capture 1.0 added. - Updated with B&R Task Manager 2.0.1. - Updated with B&R VNC Viewer 3.10. - Updated with B&R Image Viewer 1.2. - Updated with B&R PVI 3.0.0.3008. - Updated with B&R PVI Demo 3.00. - Updated with B&R Server Applet 3.7. - SNTP settings fixed: trustlocalclock = 0. - SDK: define BR_PP300_400 added. - The USB drivers (EHCI.DLL and USBDISK6.DLL) have been updated with all Microsoft QFEs up to march 2009 (Update 090331_2009M03). - The hidden FAT file system now supports partitions with less than 16MB (FAT12, ID=0x11). ------------------------------------------------------------------ Version V1.1 / 2008-10-27 / HOH ------------------------------------------------------------------ Fixes BSP: - The screen saver did not start after a reboot. - During touch screen calibration the "touch timeout" was decreased. Solved with ELO touch screen driver V1.16. - Sometimes the START.DAT keyword STORAGEMEMORY was not handled correctly. Solved with B&R AutoRun V4.6. Image: - ID 185075: The SIP could not be started in the power-On password dialog. - ID 179375: Time synchronization did not work over SNTP between two Windows CE devices. Solved with corrected SNTP settings in the registry: "trustlocalclock" = 1. - ID 152370: Empty string in SETTINGS.REG caused a crash. Solved with B&R AutoRun V4.6. - B&R PP300/400 CE6.0 SDK V1.0 and B&R PPC300 CE6.0 SDK V1.0 could not be used together. Solved with new platform ID of the B&R PP300/400 CE image. - The B&R WinCE RDP client did not work. Solved with corrected RDP settings in the registry: [HKEY_CLASSES_ROOT\MsTscAx.MsTscAx.3] changed to [HKEY_CLASSES_ROOT\MsTscAx.MsTscAx.6] - The B&R desktop logo was too large for QVGA resolution. - The power-On password dialog was too large for QVGA resolution. Changes BSP: - Updated with BIOS loader V2.3: * The loader checks if there is enough free RAM (default: > 96 MB) available to start the B&R Windows CE image. The amount of required RAM can be set with the new START.DAT keyword "RAMMIN=". * The loader displays a startup message if the START.DAT keyword ERRORMSG=1 is set. * The loader is now based on the source code of Windows Embedded CE 6.0 R1. - Updated with B&R control panel applet Server V3.5. This version supports the creation of a telnet default user. - Updated with B&R control panel applet Touchscreen V3.6. - Updated with QFE 071030_KB942494 (for USB drivers). - Updated with B&R Set Date & Time utility V1.6. - Updated with B&R screen saver SSBlank V1.3. - Updated with B&R screen saver SSFloat V1.2. - The escape codes DISPLAY_ON and DISPLAY_OFF were implemented in LxVideo.dll. Image: - "Alphablend API (GDI Version)" component added. This component is required for display of transparent GIF and PNG images. - "Simple Network Management Protocol (SNMP)" component added. - B&R Task Manager V1.1 added. - B&R Image Viewer V1.1 added. - Updated with following Windows CE 6.0 updates: * Windows Embedded CE 6.0 Update 080229_2008M02 * Windows Embedded CE 6.0 Update 080331_2008M03 * Windows Embedded CE 6.0 Update 080430_2008M04 * Windows Embedded CE 6.0 Update 080531_2008M05 * Windows Embedded CE 6.0 Update 080630_2008M06 * Windows Embedded CE 6.0 Update_080731_2008M07 * Windows Embedded CE 6.0 Update 080831_2008M08 * Windows Embedded CE 6.0 Update 080930_2008M09 - Updated with B&R VNC Viewer V3.6.5. - Updated with B&R PVI V2.6.0.3008. New: Modbus Linie. - Updated with B&R Registry Editor V3.4. - Updated with B&R ADI driver V1.24. ------------------------------------------------------------------ Version V1.0 / 2008-03-20 / HOH ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------