------------------------------------------------------------------ File: Readme.txt Version: V1.2 Date: 2009-05-04 Description: B&R Windows CE 6.0 PP300/400 ------------------------------------------------------------------ Below you will find a short description and version information of the software. ------------------------------------------------------------------ Version V1.2 / 2009-05-04 / HOH ------------------------------------------------------------------ Changes - Execution time of large applications improved. - Component XML Mime Viewer added. - XML files associated with Internet Explorer. - Component PCL Printer Driver added. - Component Animation Control added. - All "Locales" added. - Used CE 6.0 updates: * Windows Embedded CE 6.0 Product Update Rollup 2008 * Windows Embedded CE 6.0 Update 090131_2009M01 * Windows Embedded CE 6.0 Update 090228_2009M02 * Windows Embedded CE 6.0 Update 090331_2009M03 - B&R Screen Capture 1.0 added. - Updated with B&R Task Manager 2.0.1. - Updated with B&R VNC Viewer 3.10. - Updated with B&R Image Viewer 1.2. - Updated with B&R PVI 3.0.0.3008. - Updated with B&R PVI Demo 3.00. - Updated with B&R Server Applet 3.7. - SNTP settings fixed: trustlocalclock = 0. - SDK: define BR_PP300_400 added. - The USB drivers (EHCI.DLL and USBDISK6.DLL) have been updated with all Microsoft QFEs up to march 2009 (Update 090331_2009M03). - The hidden FAT file system now supports partitions with less than 16MB (FAT12, ID=0x11). ------------------------------------------------------------------ Version V1.1 / 2008-10-27 / HOH ------------------------------------------------------------------ Fixes BSP: - The screen saver did not start after a reboot. - During touch screen calibration the "touch timeout" was decreased. Solved with ELO touch screen driver V1.16. - Sometimes the START.DAT keyword STORAGEMEMORY was not handled correctly. Solved with B&R AutoRun V4.6. Image: - ID 185075: The SIP could not be started in the power-On password dialog. - ID 179375: Time synchronization did not work over SNTP between two Windows CE devices. Solved with corrected SNTP settings in the registry: "trustlocalclock" = 1. - ID 152370: Empty string in SETTINGS.REG caused a crash. Solved with B&R AutoRun V4.6. - B&R PP300/400 CE6.0 SDK V1.0 and B&R PPC300 CE6.0 SDK V1.0 could not be used together. Solved with new platform ID of the B&R PP300/400 CE image. - The B&R WinCE RDP client did not work. Solved with corrected RDP settings in the registry: [HKEY_CLASSES_ROOT\MsTscAx.MsTscAx.3] changed to [HKEY_CLASSES_ROOT\MsTscAx.MsTscAx.6] - The B&R desktop logo was too large for QVGA resolution. - The power-On password dialog was too large for QVGA resolution. Changes BSP: - Updated with BIOS loader V2.3: * The loader checks if there is enough free RAM (default: > 96 MB) available to start the B&R Windows CE image. The amount of required RAM can be set with the new START.DAT keyword "RAMMIN=". * The loader displays a startup message if the START.DAT keyword ERRORMSG=1 is set. * The loader is now based on the source code of Windows Embedded CE 6.0 R1. - Updated with B&R control panel applet Server V3.5. This version supports the creation of a telnet default user. - Updated with B&R control panel applet Touchscreen V3.6. - Updated with QFE 071030_KB942494 (for USB drivers). - Updated with B&R Set Date & Time utility V1.6. - Updated with B&R screen saver SSBlank V1.3. - Updated with B&R screen saver SSFloat V1.2. - The escape codes DISPLAY_ON and DISPLAY_OFF were implemented in LxVideo.dll. Image: - "Alphablend API (GDI Version)" component added. This component is required for display of transparent GIF and PNG images. - "Simple Network Management Protocol (SNMP)" component added. - B&R Task Manager V1.1 added. - B&R Image Viewer V1.1 added. - Updated with following Windows CE 6.0 updates: * Windows Embedded CE 6.0 Update 080229_2008M02 * Windows Embedded CE 6.0 Update 080331_2008M03 * Windows Embedded CE 6.0 Update 080430_2008M04 * Windows Embedded CE 6.0 Update 080531_2008M05 * Windows Embedded CE 6.0 Update 080630_2008M06 * Windows Embedded CE 6.0 Update_080731_2008M07 * Windows Embedded CE 6.0 Update 080831_2008M08 * Windows Embedded CE 6.0 Update 080930_2008M09 - Updated with B&R VNC Viewer V3.6.5. - Updated with B&R PVI V2.6.0.3008. New: Modbus Linie. - Updated with B&R Registry Editor V3.4. - Updated with B&R ADI driver V1.24. ------------------------------------------------------------------ Version V1.0 / 2008-03-20 / HOH ------------------------------------------------------------------ - First Version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Straße 1 A - 5142 Eggelsberg Tel: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------