------------------------------------------------------------------ File: Readme.txt Version: V5.1 Date: 27.07.2006 Description: WinCE5.0 PP100/200,MP100/200 ------------------------------------------------------------------ This file contains a short description and version information regarding the delivered software. ------------------------------------------------------------------ GENERAL INFORMATION ------------------------------------------------------------------ ------------------------------------------------------------------ Version V5.1 / 7/27/2006 / KEP ------------------------------------------------------------------ - A&P 144230: Sometimes the MCX is not initialized on the Mobile Panel - Keys does not work The Automation Device Interface 2.01 fixes this problem (see A&P 138580) - A&P 143945: Integration of the QFE package Update 060630_2006M06 This update has been integrated. - A&P 142085: Integration of the QFE package "May 2006" This update has been integrated. - A&P 14770: Remove LMemDebug LMemDebug was removed. - A&P 139260: Telnet server enabled after restart If the Web server is enabled in the Server applet in the Control Panel, it and the Telnet server are active after restarting. This problem has been corrected. - A&P 138890: Cannot create C++ MFC Smart Device applications with the B&R Windows CE 5.0 Power Panel SDK The error message "Invalid procedure call or argument" appeared when attempting to create a Visual C++ application with Visual Studio 2005 and the B&R Windows CE 5.0 Power and Mobile Panel 100/200 SDK 5.0. This problem have been corrected with Version 5.1 of the SDK. - A&P 138580: ADI update Automation Device Interface 2.01 has been integrated. This version corrects the following problems: A&P 137210: The B&R Control Center no longer recognizes the B&R Windows CE device if "Keyboard repeat" was disabled in the Control Panel. A&P 127940: Error correction for key no. 121 - A&P 135475: Function for cleaning the touch screen The "Screen cleaning" function has been implemented in the Touch Screen applet in the Control Panel. - A&P 135470: INI files should be linked with PWord INI files are now linked to PWord. - A&P 131915: "Remote Desktop Active X Control Interface" not completely implemented The "Windows RDP Control" has been replaced by teh "ActiveX RDP Control". - A&P 128990: SCRSAVE.EXE should only be started once AUTORUN.EXE has ended. This behavior has been implemented. - A&P 128545: Integration of the QFE package "Q3 2005" This update has been integrated. - A&P 139850: Integration of Windows CE 5.0 update 060430_2006M04 This update has been integrated. - A&P 128455: Saving the registry on restart The Configuration Manager applet in the Control Panel saves the registry before a restart. - A&P 123895: Default interface for the PVI demo The serial interface has been changed to COM1. - A&P 123890: The Server applet should enable the integrated server without restarting The Server applet in the Control Panel now enables and disables the server without needing to restart the B&R Windows CE device. - A&P 135155: Windows CE for PP deletes Extended CMOS B&R Windows CE deletes the model number of an aPCI module in Slot 1. This problem has been corrected. ------------------------------------------------------------------ Version V5.0 / 28.07.2005 / KEP ------------------------------------------------------------------ - First version. ------------------------------------------------------------------ Copyright (c) by B&R ------------------------------------------------------------------ Bernecker + Rainer Industrie-Elektronik Ges.m.b.H. B&R Strasse 1 A - 5142 Eggelsberg Tel.: +43 (0)7748/6586-0 Fax: +43 (0)7748/6586-26 Email: office@br-automation.com Web: http://www.br-automation.com ------------------------------------------------------------------