B&R Logo
  • Website
  • Model Number
  • Serial number
Login
Logged in as UsernameLogout
Loading...
English International

Please choose your country:

Boosting machine availability through condition monitoring

STOCK_Schraubenschlüssel-2

From oscilloscope modules to sensor-equipped servo drives, from the monitoring chip inside every Automation PC to vibration analysis modules with embedded intelligence, B&R offers every possibility to keep your finger on the pulse of the machine without requiring any external units. Condition monitoring is already an integral part of every B&R system and consequently of every machine that is automated with B&R technology. Predictive maintenance based on constant condition monitoring helps avoid unplanned downtime and reduces the cost of stocking spare parts. Using condition measurements as input for open and closed control loops can significantly increase the service life of a machine and contribute to substantially reduced unit costs.

The development efforts of mechanical engineers in machine manufacturing are paying off as the power density and functional density of production machines continue to increase. This means that fewer machines are required to produce the same quantity and complexity of products, which lowers production costs and makes machine manufacturers more competitive. On the other hand, this increased efficiency also makes producers more dependent on individual machines. The ability to produce more units per hour means that each hour of downtime is more expensive. And anyone who has ever operated a machine knows that downtime can never be completely avoided.

Rethinking maintenance strategy

Traditional maintenance strategies have one thing in common: Those last few percentage points in machine availability come at a high price. This is true for reactive, damage-oriented maintenance, where a system's components are driven to exhaustion and only replaced when they fail. The only way to ensure machine availability in this scenario is to maintain a stock of replacement parts and have qualified personnel and the necessary equipment available on short notice. The most widespread traditional strategy, however, is preventive maintenance at fixed intervals based on experience. Although this approach has the distinct advantage of making maintenance downtime more plannable, it is certainly no cure-all and involves considerable financial risk. On the one hand, you have parts being purchased and replaced although the originals are far from the end of their useful life. On the other, you have no reliable protection against unplanned downtime, such as when asymmetric strain causes certain parts to fail prior to the maintenance interval.

Minimizing downtime as much as possible and crafting a strategic plan for maintenance that can't be avoided – these are the goals of any responsible machine operator who not only looks at the purchasing price when evaluating new machines, but also at the overall costs over their entire useful life. The only way to significantly impact the total cost of ownership is to maximize machine uptime while simultaneously minimizing maintenance costs. Which in turn requires a rethinking of traditional maintenance strategies.

Machine-dependent preventative maintenance

The best way to optimize the ratio of machine availability to maintenance costs is to replace the fixed maintenance intervals with condition-dependent, predictive maintenance. This involves scheduling maintenance when changes in monitored parameters indicate impending failure. The advantage of this is that components can continue to provide value until much closer to the actual end of their useful life, which is typically much later than the conservatively estimated maintenance interval. Yet there is no sacrifice in plannability since the required maintenance can be performed during regularly scheduled breaks in production. The risk of maintaining a stock of replacement parts is also minimized since only the affected components need to be replaced. This is also a way to reliably avoid failures that result from neglected maintenance.

For any of this to be possible, condition parameters throughout the machine must be monitored constantly, and this data must be evaluated correctly to determine which parts require maintenance. "This can be based on simple signals and measured values such as temperature or pressure that are collected using X20 or X67 I/O modules," explains Bernhard Eder, business manager at B&R. "On top of that, B&R also offers specialized modules such as valve control modules with integrated switching time detection or oscilloscope functions."

Countless other options for monitoring condition signals are natively integrated in B&R automation systems. These include ACOPOS servo drives with built-in motor monitoring, for example, as well as B&R Automation PCs, which are equipped with an integrated circuit for seamless self-diagnostics. The latest addition to this selection is a new module in the X20 series for vibration analysis.

"The sensor technology used to obtain the signals is indeed important, but the sensors alone are not enough," explains Werner Paulin. Paulin has gained years of international application experience since he joined the company in 1997 and is currently B&R's international sales manager for China. "The key to scheduling maintenance on time, but not too early, is correct interpretation of the recorded signals. That's the only way to accurately predict developing problems."

Schema-CM-Modul

An optional feature becomes standard

This is why condition monitoring – which in fact has been around for decades – has been slow to take hold in traditional machine manufacturing. The complex mathematics involved have typically required large and expensive dedicated computer systems, which in turn needed to be programmed by experts in fields such as material science and vibration mechanics. Because of this, condition monitoring was limited to systems whose failure would result in immense costs.

The shrinking scale of microelectronic components has since eliminated the need for expensive external wiring. B&R's analog input module X20AI2636, for example, comes standard with essential functions such as a comparator with hysteresis. The X20CM4810 condition monitoring module from B&R, which is currently being implemented at selected pilot customers, converts signals read from the acceleration sensors into more than 70 specific values. This allows even complex vibration patterns to be monitored.

Developers can easily configure which factors should be monitored in B&R Automation Studio without requiring knowledge of complex mathematical functions, which solves a lot of problems with regard to software and interfaces. At runtime, significant values are sent to the system CPU via POWERLINK and can then be applied directly in the application software. "For the first time, machine manufacturers are able to offer condition monitoring not as a premium option, but as a fully integrated standard feature," states Paulin emphatically. "As a result, they can give their customers availability guarantees with considerably lower imputed risk."

ipad SDM

Longevity is part of the package

Machine operators can also benefit from the integration of condition monitoring with a company's internal logistics systems. When the machine identifies the need for maintenance, for example, it can automatically trigger a reminder to the maintenance or purchasing department for the required parts. This prevents orders from being overlooked or placed incorrectly and ensures that the right part is on hand when it is needed without having to maintain a large stock on site.

Maintenance isn't the only area where having live, preprocessed condition data opens up new possibilities, however. Recorded condition data can also be fed into the automation software to provide additional functionality. "This allows you to adjust the speed in order to extend the time before maintenance, for example, or to compensate for slack or switching delays in order to maintain optimal operating conditions," says Eder. "This kind of adaptive operation can further contribute to increased availability and a longer service life – which in the end means more efficient resource utilization and lower unit costs."

Paulin Werner

"A machine's service life and availability can be increased significantly by 'putting your ear to the tracks' to adapt operation and schedule maintenance. "Aside from mechanical vibration, B&R continues to offer a wide selection of options for recording and evaluating signals to respond to the current condition of individual machine components." Werner Paulin, International Sales Manager - China

BuR_Eder 4

"You pay a high price for those last few percentage points in availability if you stick to traditional maintenance strategies. "This price can be drastically reduced using predictive strategies based on permanent condition monitoring." Bernhard Eder, Business Manager - Customized Solutions

'

Agreement concerning the use of images

\

Important information concerning the use of image material


\

The act of copying or in any way using the image linked below indicates that you have read and understand the following agreement concerning the use of images, which governs the usage of image material. If you do not accept the conditions of agreement, then you are not permitted to copy or to use the image in any capacity, without written consent from B&R.

\

User agreement:


\

In accordance with the conditions of this agreement, the image is only available for editorial purposes for members of the press or industry specialists. Right of use is limited to you only and cannot be transferred to third parties. The image may not be used to advertise or sell any product or technology (e.g. usage in advertisements, brochures, book covers, image databases, t-shirts or other promotional material). The image may not be altered or modified in any way, as a whole or partially. B&R is and remains at all times the sole owner of the image. You are not permitted in any way to delete, alter or conceal any legends or descriptions belonging to the image.

\

B&R provides the image as is and without any guarantees. You, not B&R, carry sole responsibility for your use of the image. B&R is either the owner or the licensee of the image and not an intermediary of the owner. By using the image material, you are inherently obligated to print "Copyright B&R" at a suitable location in the publication. Furthermore, a sample copy of any printed publication containing the image must be sent to B&R.

';
Share
This site uses cookies to enable a better customer experience. By continuing to browse the site you are agreeing to our use of cookies. Please find more information about cookies in our Data privacy statement.